Murrelektronik

You are here: Murrelektronik – stay connected / Selskap / Miljø

Miljøvern

Bærekraftig utvikling og beskyttelse av naturen

Murrelektronik is committed to the objectives of environmental protection. Special emphasis is given to the protection of employees and customers. This begins with the selection of raw materials: no material hazardous to health is used for the production of Murrelektronik products, as prescribed by the Dangerous Substances Directive. Lead-free production is of special importance: Murrelektronik follows the guidelines of the RoHS directive. This is also taken into account when selecting suppliers.

The very modern production facilities are designed to use less energy. Environmental criteria are also considered for shipping our goods. Only recyclable materials, such as polythene wrap and cardboard boxes are used as packing material.

Internasjonale representanter

Internasjonale representanter

Murrelektronik verdsetter forbindelser. Du vil finne kunnskapsrike medarbeidere i våre lokale avdelinger og internasjonale kontorer.

Mer