You are here: Murrelektronik – stay connected / Nyheter / Produktnyheter / Detail page


21. april 2017

“In the final analysis, overall costs are less”

With Mico Pro®, the potential distribution concept is already integrated. Murrelektronik Product Manger Tobias Berner explains the benefits of this solution.

Tobias Berner, Product Manager Power Distribution

Mr. Berner, what advantages does the integrated potential distribution concept have? It allows potential groups to be built and several consumers to be connected directly. This decentralizes installations in the control cabinet and reduces the expenditure for wiring. In the final analysis, overall costs are less.

How is potential distribution implemented specifically? Mico Pro® has at each output a 24-volt terminal as well as a connection option for zero potential. The use of potential distributor modules multiplies the number of monitored outputs. Since they are already supplied with 0 V through the bridge system, it is enough to run a wire from one monitored output to any positive contact of the potential distributor module. This offers maximum flexibility.

How does this affect the space in the control cabinet? We have customers who have saved up to 80 percent of space. Entire terminal strips, which require a lot of space, are not needed.

Are there other advantages? The installation becomes very organized. The entire Mico Pro® system has a plug-in design. This saves about 75 percent of the time needed for installation. During operation, this technology is also completely maintenance free and vibration resistant.

Mico Pro in Murrelektronik's Online Shop